请输入产品型号或部分型号。
Please refer to my Murata. We have the detailed information on the schematics, etc. The Pin is 50 ohms, but, there can be antenna tuning network which customer might implement. There is also reference antenna information that customer should use.
Return to LoRa Module Page
Back to LoRa FAQ List
请配合完成FAQ改善问卷。FAQ对您有帮助吗?
如果可以的话,请您提出对FAQ的意见及要求。您的意见将会用于FAQ的改善中。
如您有产品相关的疑问,请点击“联系我们”进行咨询。