LoRa FAQQIn the datasheet, "STSAFE" chip option for this module has been mentioned. What is STSAFE option? How can I control it? Does this mean that "STSAFE" is optional or it is an option included in the module? What is the part number of the module?

A

The module have a space for STSAFE chip inside the module. If you want to have STSAFE chip inside the module, please contact with STMicroelectronics for STSAFE chipset first.
Once you fix the contents of STSAFE with STMicroelectronics, please contact Murata.
There is minimum volume requirement for this option.

Return to LoRa Module Page

Back to LoRa FAQ List

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。