Select your region & language

Murata introduces Hybrid multiplexer for smartphone wireless circuits

  • Acoustic Wave Device

19/04/2017

Murata Manufacturing Co., Ltd.
President/Statutory Representative Director:
Tsuneo Murata

Overview

Murata Manufacturing Co., Ltd. has developed the LMTP3P series of hybrid multiplexer for smartphones. This product can branch to three frequency bands, and therefore it reduces the number of antennas and contributes to device size reduction when used with a wireless circuit. Steep attenuation and wide band transmission are achieved with Murata original technology that combines the properties of a multilayer ceramic and a SAW filter.  Mass production of the hybrid multiplexer began this April.

Background

Carrier aggregation*1 and MIMO*2 antenna systems are being increasingly adopted in LTE*3 communications in order to improve communications speeds for smartphones. With LTE, the communication frequencies are divided to low band (698~960MHz), middle band (1427~2200MHz) and high band (2300~2690MHz). With carrier aggregation, which simultaneously uses multiple frequency bands, an antenna is generally required for each frequency band. MIMO systems, which improve communications speed by using multiple transceiving antennas, are also being used, but they increase the quantity of required antennas and make the wireless circuit more complex.
The hybrid multiplexer launched by Murata at this time can branch to the three frequency bands, thereby reducing the number of antennas needed for carrier aggregation. This provides design surface area for MIMO systems that require multiple antennas, and can contribute to size reduction for a device.

Features

  • Able to use a passive circuit to divide low band (698~960MHz), middle band (1427~2200MHz) and high band (2300~2690MHz).

  • Supports LTE and GMS transceiver applications
  • Dimensions (mm): 3.5 (L) x 3.5 (W) x 0.9 max

Part number

LMTP3PAA-J63

Explanation of terms

*1. Carrier Aggregation is technology that improves communications speed by simultaneously using multiple LTE carrier waves. Intra-Band Carrier Aggregation uses the same frequency band while Inter-Band Carrier Aggregation uses differing frequency bands.
*2. MIMO stands for Multiple-Input and Multiple-Output, a technology that improves communications speed by using multiple transceiving antennas. LTE is starting to be used in wireless LAN.
*3. LTE stands for Long Term Evolution, classified as the fourth-generation communications method (4G), and its use enables high speed communication for mobile phone networks.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter