Select your region & language

Silicon capacitor supports new power distribution networks performance requirements

  • Capacitor

18/06/2021

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Murata has extended its product offering for the mobile and high-performance computing (HPC) markets with the availability of its latest silicon process technology to fabricate silicon capacitors with a density of 1.3µF/mm². The extremely low ESL (few pH) and low ESR (few mΩ) of these devices support the highest performances of new power distribution networks (PDN) that require low impedance over a wide frequency bandwidth.

As digital ICs evolve to offer more features at lower voltages, resolving issues like noise and voltage fluctuation is critical. Its <40µm profile enables chip designer engineers to embed the silicon capacitor into the package as close to the active die as possible, minimizing the current’s effective path length and, thereby, minimizing parasitics.

These multi-terminal devices satisfy the various SoC and microprocessor design requirements for multiple terminal capacitor networks. Replacing conventional monolithic ceramic capacitors with multi-terminal silicon devices reduces the total quantity of capacitors required on the board significantly, which improves the compactness of the end design. Fewer capacitors also results in total savings in both bill of materials and mounting costs.

About the silicon capacitors

Please click here for the product details.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter