Select your region & language

Murata Manufacturing commercializes a compact wireless module with built-in MCU, that can be easily incorporated into other products - New product to help bring IoT devices earlier to market -

  • Connectivity Modules

08/06/2022

Murata Manufacturing Co., Ltd. (hereinafter, "Murata") has developed "Type ABR," a compact wireless module containing a built-in wireless micro-controller ("88MW320") from NXP semiconductors N.V (hereinafter, "NXP"). Mass production has already started for "Type ABR."
The speed at which products and services are developed has become increasingly important in recent years, with the rapid growth of the IoT market. However, providing products with wireless communication functionality has until now required some degree of familiarity with Wi-Fi™ and other wireless communication technologies, and this has increased the time it takes to develop products. There is therefore a growing demand for communication modules that can make it easier to implement wireless functionality.
In response, Murata has developed Type ABR as a solution to enable Wi-Fi functionality just by entering some simple commands. It is compliant with the Radio Act, so there is no need to obtain separate certification. It also contains a built-in NXP MCU, allowing it to be used with software development tools (EZ-Connect™, WMSDKA) that use the NXP framework for simplifying application development. This can reduce the amount of resources spent on design, allowing IoT devices to be brought more quickly to market.

Specifications

  • Simple implementation helps to reduce the amount of resources spent on design
    • The Wi-Fi module built into the MCU allows for Wi-Fi functionality to be added just by entering some simple commands.
    • It contains an integrated antenna for excellent RF performance without any need to prepare a separate antenna.
  • Compliant with the Radio Act
    • Type ABR is compliant with the Radio Act, so there is no need to obtain separate certification.

Specifications

Part Number CMWC1ZZABR
Type Name Type ABR
IC Manufacturer NXP
Chipset 88MW320
Technology Wi-Fi
Wi-Fi Wi-Fi 4
Frequency 2.4GHz
Bluetooth® No
Integrated Antenna Yes
Dimension 22 × 19 × 2.4 mm
Supply Voltage 3V to 3.6V
Interface Voltage 3.3V
FCC/IC Certified Yes
ETSI Report Yes
MIC (Japan) Certified No
Operating Temperature (degC) −30°C to 85°C
Mounting Type SMT

Product pages

Check "Type ABR" for product details.

Inquiries

Access this page to send an inquiry on "Type ABR."

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter