Select your region & language

Murata Launches World’s Smallest RF / Microwave Coaxial Connectors with a Switch, Cutting PCB Mounting Area by Approximately 40%

  • Connectors

29/10/2026

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

​

Murata Manufacturing Co., Ltd. has begun mass production of the SWL series MM8330-2600RJ5 and MM8330-2600RK20, the world’s smallest RF / microwave coaxial connectors with a switch*. Measuring just 1.0 mm × 1.0 mm × 0.55 mm, the new connectors reduce PCB mounting area by approximately 40% compared with Murata’s previous SWJ series. When used with dedicated probes, the SWL series reduces its PCB footprint, including the keep-out area, by approximately 60% compared with Murata’s previous SWJ series.

As wireless devices incorporate more functionality, rising component counts are placing increasing pressure on limited PCB space. RF test connectors require not only mounting area for the connector itself, but also sufficient clearance around the component for probe access during circuit measurement.

How RF Signals Are Measured Using a Coaxial Connector with a Switch and a Probe RF Signal Measurement Using a Coaxial Connector with a Switch and a probe

Reducing the Space Required for RF Measurement

Murata addresses these constraints with a proprietary structure that combines its RF and mechanical design technologies. The design achieves miniaturization while maintaining low RF transmission loss and mechanical robustness. At 1.0 mm × 1.0 mm × 0.55 mm, the SWL series is smaller than Murata’s previous SWJ series, which measures 1.4 mm × 1.2 mm × 0.65 mm, allowing greater flexibility in PCB component placement.

When used with the dedicated automatic or manual probe, the connector requires less clearance around the test point, reducing the total board area required for RF measurement. The dedicated probes are scheduled to enter mass production in December 2026.

Comparison of Mounting Area and Occupied Area Between the New SWL Series and Previous SWJ Series Murata’s SWL Series Reduces PCB Mounting Area by Approximately 40% and Probe-Related Occupied Area by Approximately 60% Compared with the Previous SWJ Series

Supporting Frequencies up to 15 GHz

The SWL series supports a frequency range from DC to 15 GHz with a nominal impedance of 50 Ω. The MM8330-2600RJ5 is supplied on reels of 5,000 pieces, while the MM8330-2600RK20 is supplied on reels of 20,000 pieces.

Murata will continue developing smaller electronic components and solutions that enable more effective use of limited PCB space, supporting higher-performance and more compact smartphones and wearable devices.

For more information, please visit the product page. For product inquiries, please contact Murata.

This video further explains the role of RF / microwave coaxial connectors with a switch and their use in circuit measurement.


  • Notes:


  • * Based on Murata research as of October 28, 2026.
​

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter