Select your region & language

Murata Releases Advanced Noise Filter Design Support Tool That Contributes to Saving Design Resources

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

07/04/2022

Murata Manufacturing Co., Ltd. (“Murata”) released the Advanced Noise Filter Design Support Tool (the “Design Tool”), which features a sophisticated software tool function that supports the selection of a noise filter.
This Design Tool enables users to freely set the target noise frequency and other conditions in detail. The enhanced automatic component selection function contributes to saving the user’s design resources. This tool is available for free on the Murata website.

When designing noise suppression, designers first measure the frequency that needs to be resolved by using actual equipment and set a target noise reduction level based on the standards at the location where the final products are going to be shipped to. When formulating a noise suppression policy, it is very useful to be able to verify the noise suppression effect while selecting components and noise filter configuration in terms of verifying how close the test models are to the target noise suppression level. Murata offers the Noise Filter Design Support Tool to answer the needs of our customers.
However, the conventional Noise Filter Design Support Tool is only capable of automatic optimal component selection for filter configuration upon initial setup. Therefore, Murata developed this new Design Tool with an additional function that automatically selects the optimal components for any filter configuration selected any time after the initial setup. This function also allows for the selection of a frequency range for considering insertion loss properties as well as taking into account the footprint of components when reviewing the filter configuration.
Murata will continue developing tools that respond to a wide variety of applications and enable the selection of optimal items from numerous noise filters, thereby saving the design resources of noise suppression designers.

Features of the Design Tool

  • Automatically calculates and displays the component combination that provides the highest noise suppression effect, with the user simply setting the conditions (Fig. 1).
  • Filter configuration can be flexibly selected while comparing several simulation patterns.
  • Any frequency range can be selected when considering insertion loss properties.
  • Multiple filter configurations can be compared using the reference display for the component implementation footprint.

[Fig. 1] Design Tool screen image

  1. Set the conditions in both (a) Conditions and (b) Circuit Configuration.
  2. Simulation results appear when the [Optimize] button is clicked.
Swipe left or right to change screens View in landscape mode
Design Tool screen image

Noise Filter Design Tool

For this tool, visit the “Advanced Noise Filter Design Tool Open in New Window ” for more information.

Operation manual

For details on how to use the tool, refer to the Operation Manual.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter