Select your region & language

Latest Wire Wound Chip Common Mode Choke Coils from Murata Exhibit Wideband Impedance Capabilities

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

13/03/2023

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

Leading electronics manufacturer Murata announces the introduction of the DLW32PH122XK2 wire wound chip common mode choke coil. AEC-Q200-qualified, this 1210 inch size (3.2×2.5mm) component is targeted at suppressing wideband common mode noise in modern automotive designs. It is of particular value when addressing the power supply line noise issues now occurring as advanced driver assistance system (ADAS) hardware connects with wide frequency band sensors and imaging equipment (such as radar, LiDAR, etc.). There are a multitude of opportunities for this coil to suppress noise in industrial and consumer devices too.

The DLW32PH122XK2 draws on Murata’s proprietary winding technology and the company’s in-depth understanding of materials science, as well as its ability to transition innovative design concepts into volume manufactured products. At 100MHz, this component exhibit 1200Ω (typical) impedance levels, and it maintains 900Ω (typical) even when 1GHz frequencies are applied. Any competing chokes operating over such an extensive range of frequencies would be substantially bigger, making them impractical in space-constrained environments.

Murata’s DLW32PH122XK2 is 60VDC rated and supports currents up to 1.2A at 105°C. It is the world's first 1210 inch size high-frequency, high-current common mode choke coil for power supply lines to handle such currents and simultaneously have effective impedances at GHz frequencies. A low DC resistance, of 0.05Ω (typical), mitigates power losses and curbs unwanted heat generation.

More information on this common mode choke coils is available here

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter