Select your region & language

Murata commercializes 0504 inch size chip common mode choke coils for use with vehicle-mounted differential interfaces (LVDS/SerDes/USB/HDMI)

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

17/12/2024

Murata Manufacturing Co., Ltd. (hereinafter, “Murata”) has newly commercialized the noise suppression products, 0504 inch size chip common mode choke coils “DLM11CN_HH2 Series (hereinafter, product)” which are suitable for use with high-speed differential interfaces used in automobiles such as LVDS*1, SerDes*2, USB, and HDMI. Mass production of this product began in December 2024.

  • *1LVDS (Low Voltage Differential Signaling): An interface used for LCD panels.
  • *2SerDes (Serializer/Deserializer): Circuits that convert between the serial and parallel signals in each direction.

In the automobile market, the development of the advanced driver-assistance system (ADAS) and autonomous driving (AD) has led to an increase in the range and number of sensing devices such as vehicle periphery sensing cameras and LiDAR*3, as well as display devices such as around view monitors, headup displays, smart rearview mirrors, and LCD speedometers. LVDS and SerDes are used for the transmission of image data in these devices. Multiple USB ports are equipped in each vehicle seat as interface for connecting smartphones and computers, which calls for smaller products. Common mode noise suppression is a key issue for these differential interfaces, and therefore a smaller common mode choke coil is in demand for high-speed signals. Drawing on proprietary lamination technique, Murata developed the 0504 inch size―smaller than the conventional 0805 inch size―as a solution to this demand.

  • *3LiDAR (Light Detection and Ranging): A system that detects obstacles around the vehicle by emitting lasers.

Specifications

Product name DLM11CN500HH2 DLM11CN900HH2 DLM11CN201HH2
Common mode
Impedance
(at 100 MHz)
45Ω±25% 90Ω±25% 200Ω±25%
Rated current 100 mA 80 mA 60 mA
Operating temperature range ‐55 to +125℃
Others AEC-Q200*4 compliant
  • *4AEC-Q200: One of the standards defined by the AEC (Automotive Electronics Council).

Product pages

Check the DLM11CN_HH2 Series for product details.

Related sites

Selection chart for signal lines: List of recommended common mode choke coils for automobiles by interface

Inquiries

For free small-quantity samples, click here for inquiries.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter