Select your region & language

New Murata Automotive-Compliant Chip Ferrite Beads Deliver Wide Band Noise Suppression of High-Frequency (5.9GHz) C-V2X

  • Noise Suppression Products / EMI Suppression Filters / TVS Diodes (ESD Protection Devices)

19/06/2025

Murata Manufacturing Co., Ltd.
President:
Norio Nakajima

The new BLM15VM series is ideal for automotive powertrains and safety applications. It supports high frequencies. 1000Ω (Typ.) @5.9GHz. With its compact 0402-inch size (1.0×0.5mm) can operate at temperatures ranging from -55 to 150°C. And it is compliant with AEC-Q200.

Murata Manufacturing Co. Ltd continues to push the envelope in automotive noise suppression technology with another industry first. By leveraging proprietary material technology and optimized structural design, the company’s new BLM15VM series of automotive-compliant chip ferrite beads deliver wide-band noise suppression of high-frequency (5.9GHz) 5G vehicle-to-everything (5G-V2X) applications that exhibit high impedance. Mass production is scheduled to begin in July 2025.

In recent years, the use of high-frequency wireless communication in the automotive sector has increased. It is primarily used for content distribution for navigation, audio and other infotainment systems. Improving sensitivity and noise suppression in these advanced high-frequency communication systems becomes mission critical to support the connected car for ADAS (Advanced Driver Assistance Systems) and eventually autonomous driving.

RF inductors typically used for noise suppression in sub-6GHz communication have a narrow frequency band at high impedance, making it necessary to select components that match the noise frequency band. With its broad high-frequency band at high impedance, the BLM15VM series allows easy noise suppression across multiple frequency bands using just one product. Even at 5.9GHz, the chip ferrite beads within the series will typically attain impedance values of 1000Ω.

By enabling error-free high-frequency communication, which is crucial for autonomous driving, the BLM15VM series significantly improves reception sensitivity in V2X communication in the 5.9GHz bands for autonomous driving and stable operation of dedicated short-range communication (DSRC) based control systems, operating in the 5.8GHz band, for improved road safety. Additionally, since Wi-Fi 6E and Wi-Fi 7, the communication standards for wireless LAN, also use the sub-6GHz band, this product can improve sensitivity and suppress noise in consumer communication devices.

The AEC-Q200-compliant BLM15VM series of chip ferrite beads from Murata supports operating temperatures between -55 to 150°C and is supplied in a compact 0402-inch size(1.0×0.5mm). Murata is committed to expanding its lineup to meet market needs.

For more details about the Product, see the ‘BLM15VM150BH1’ page.
Requests of free small-quantity samples are available here.
For inquiries regarding the product, click here.

Editor’s Notes

According to the Company's research. This is the world's first product that removes noise in high-frequency communication (including Sub6 bands) for C-V2X, as of June 18,2025.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world.

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter