Select your region & language

New wire-wound inductors for car cameras and NFC circuits

  • Inductors

22/07/2016

New wire-wound inductors for car cameras and NFC circuits

Overview

Murata introduces LQW15CN_0Z/1Z series of AEC-Q200-compliant wire-wound inductors, ideal for automotive camera applications and NFC circuits

  

Background

In anticipation of the self-driving cars of the future, there has been an increase in development of on-board equipment aimed at enhancing vehicle driving and safety systems. This state of affairs has driven demand for smaller, higher-performance high-frequency inductors to be used for RF circuit matching and choke coils in vehicle-mounted equipment. To meet this demand, Murata Manufacturing Co., Ltd. has been focusing on the development of high-frequency inductors for automotive applications.

Murata's new LQW15CN_0Z/1Z series is a line of AEC-Q200-compliant wire-wound inductors for the automotive market. This inductor takes advantage of physical characteristics that make it possible to obtain large inductance in a small size, and designers can use it to efficiently configure the BiasTee circuits used in vehicle-mounted cameras. (Click here for detailed examples of applications using this product.)

The product can also be used for NFC matching circuits, which benefit from the low loss characteristics that are a feature of winding type inductors. As an automotive version of an inductor with a proven track record in general consumer applications, it can be used with confidence in on-board NFC circuits.

  

Features

  • Achieves large inductance in a compact 0402 size (1.0x0.5mm) using a ferrite core
  • Achieves large rated current and low DC resistance characteristic of wire-wound inductors
  

Applications

BiasTee circuits for vehicle-mounted cameras 
Automotive NFC circuits

  

Parts List

LQW15CN_0Z series
Click here for details of the series lineup.

LQW15CN_1Z series
Click here for details of the series lineup.

 

Production

Mass Production 

Terminology

 BiasTee circuit: A circuit with a 3-port structure used to separate the DC and AC components from the high-frequency signal, or conversely to supply the DC bias to the AC signal. The word "tee" in the name comes from the T-shape of the circuit design.



Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter