Select your region & language

Max. 0.6 mm high, Max. 22 uH power inductor for wearable devices

  • Inductors

05/04/2017

Overview

Murata Manufacturing Co., Ltd. introduces a 1008-inch (2.5 x 2.0 mm) winding power inductor for wearable devices that achieves a large L (22 uH) in spite of its low 0.6 mm profile.

  

Background

There is an increasing demand for compact, low-profile power inductors in electronic devices such as wearable devices and smart cards. Because liquid crystal panels are mounted on these devices, inductors that have both a low profile as well as a high L value are needed for the panel drivers. Yet, in the conventional monolithic type low-profile high-power inductors LQM_CH series, the L value was limited to 2.5 uH.

This is why Murata has released the 1008-inch (2.5 x 2.0 mm) winding inductors LQH2HPN_DR series intended for wearable devices. It is available in a variety of L values up to 22 uH, in spite of its low profile.

  

Features

  • Low profile ideal for wearable devices (max. 0.6 mm)
  • Wide inductance lineup (0.47uH to 22uH)
  

Applications

Power inductors for compact electronic devices such as wearable devices

  

Parts List

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter