Select your region & language

Introduction of small 0603 (1608 metric) size Metal Alloy inductors with reduced DC resistance

  • Inductors

14/09/2017

DFE18SBNR47ME0# has been discontinued.
DFE18SBN1R0ME0# is not recommended for new design (NRND).
(*Updated on Apr 1, 2024)

DFE18SBN_E0

Overview

Murata Manufacturing Co., Ltd. has introduced the DFE18SBN_E0 series of Metal Alloy inductors for the power supplies of mobile devices such as smartphones. This series offers the world’s smallest Metal Alloy power inductor, having lower Rdc*1  than former products. This product entered mass production in April of 2017.

  

Background

As mobile devices continue to implement higher density and greater performance, the market requires a small-sized power inductor that can support a large current. For this reason, Murata has made unique improvements to the metal magnetic material, thereby reducing the Rdc in comparison to the former DFE18SA series, while maintaining DC superimposition characteristics. (The DFE18SA series has Isat*2  =2.0A, Rdc=144mΩ@1uH, while the new DFE18SBN_E0 series has Isat=1.9A, Rdc=120mΩ@1uH.)

   *January 9th、 2018 Changed specifications of DFE18SBN_E0


Terminology

*1  Rdc: DC resistance
*2  Isat: Rated current based on change in inductance




Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter