Select your region & language

Murata introduces compact, high-current 0806 size Metal Alloy inductors for automotive

  • Inductors

17/01/2018

Overview

Murata Manufacturing Co., Ltd., has added the 0806-inch size (2.0 × 1.6 mm) DFE201612PD series to its DFE_PD series of Metal Alloy inductors. Suitable for the power supply of automotive information equipment such as infotainment systems, this product conforms to AEC-Q200 and supports a maximum operating temperature of 125°C. It achieves a rated current of 2.2A (at 1μH), or approximately twice the rated current of 1.0A (at 1μH) for a ferrite multilayer base power inductor of the same size(*1). Mass production of the product has already started.

  

Background

Digital and information equipment were mainly used in the consumer market, but are also now mounted in automobiles. As a result, Demand is increasing for compact, high-current power inductors used in information electronics in automotive applications which higher reliability. Therefore, Murata has modified its DFE201612P series of compact, high-current power inductors to realize a maximum operating temperature of 125°C, and has introduced the DFE201612PD series of power inductors that also supports AEC-Q200. Going forward, Murata plans to further expand its lineup of sizes and develop highly reliable inductors that can support high temperatures and high currents for automotive applications.

  

Site URL for the product

Terminology

AEC-Q200:A reliability standard for automotive electronic components

*1 Murata product LQM2MPZ_G0 series


Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter