Select your region & language

Murata Develops Wireless Power Transfer Technology Which Receives Higher Power for Electronic Cards

  • Others

09/12/2021

Murata Manufacturing (hereinafter, "Murata") has developed a wireless power transfer technology (hereinafter, "this technology") which receives higher power from an NFC reader terminal for electronic cards such as fingerprint authentication cards. Murata has already started to provide this technology as a technology solution.

In recent years, the need for fingerprint authentication cards has increased against a backdrop of improvements in personal authentication and contactless card security. Fingerprint authentication cards need a power receiving function from the NFC reader to supply power to the fingerprint sensor in the card in addition to a conventional communication function with the NFC reader terminal.

Accordingly, Murata developed this technology to receive higher power from an NFC reader terminal. With this technology, cards can receive 1.7 times power* from an NFC reader terminal compared to typical power transfer technologies. This technology enables a fingerprint authentication card to be used at a distance from NFC reader terminals even if the card is not equipped with a battery and, also helps reduce the time required for fingerprint authentication. This technology is an effective way to achieve not only fingerprint authentication cards, but also electronic cards equipped with display, sensing, communication, and other features.

  • *Comparison performed under conditions with the card placed at a distance of 4 cm from the NFC reader terminal. The results may differ depending on card distance and the type of NFC reader terminal.

Going forward, Murata will continue to strive to develop technologies to meet market needs and contribute to the shift to high-functionality and diverse electronic devices.

Higher power receiving (this technology)

Image of this product

Lower power receiving

Image of conventional product

Contact Form

Click here for inquiries regarding this technology solution.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter