Murata broadens ultra-compact, high-efficiency DC-DC converter offerings

  • Power Products

12/05/2021

Murata has introduced several new non-isolated DC/DC converter lines for distributed power architecture applications. The UltraBK™, MonoBK™, and PicoBK™ series were developed to provide small size, high efficiency, decreased noise, low EMI, and take up less board space. These products address the design challenges impacting today’s communication, storage, and server applications along with the exacting demands of the emerging 5G market.

The newest is the UltraBK™ line and comprised of the MYTNA and MYTNC series. In addition to the benefits listed above, both use patented technology to provide an ultra-thin package with industry leading efficiency. The two stage architecture systems integrate Murata’s charge pump technology with conventional DC/DC converter circuits. The result is unsurpassed package density and reliability levels. Products include both 4A and 6A models.

The expanded MonoBK™ series now includes the MYMGK-H line. Featuring high-heat resistance, it drastically cuts down on both board space and design time. Proprietary packing technology allows for internal temperature reduction with densely mounting components and by leveraging a structure that allows heat to escape from the module substrate. Products include 12A and 20A models.

Finally, the PicoBK™ low-power offering integrates an inductor with a control IC for applications where space is at a premium, such as with wearable devices. These very small modules have low quiescent current which is preferred for battery powered applications. Products include 0.5A, 1.0A, 1.5A and 2.0A models.

More information can be found here.

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter