Select your region & language

Compact, cost efficient DC panel meters ease interface challenges

  • Power Products

12/11/2019

Compact, cost efficient DC panel meters ease interface challenges

Murata is introducing a new panel meter series developed by Murata Power Solutions for industrial applications. Comprised of several models, the DMR30 Series offers the ability to measure DC voltage, DC current, temperature, various process voltages, or current loop’s commonly used in industrial processes. All meters are powered through a 9-32VDC external source and configured via a touch-panel user interface. They are designed to fit in a 2” round mounting hole.

The DMR30-DCV1 model is a Voltmeter that provides DC voltage measurement ranges of 200mV, 2V, and 20V and has 4.5 digits of resolution. The DMR30-DCA1 is an ammeter that provides DC current measurement ranges of 1A - 1200A when used with industry-standard external shunt resistors (50mV and 100mV output types) and up to 3.5 digits of resolution. The DMR30-PM1 Process Meter performs precision process signal measurements supporting 0-5V and 0-10V voltage and 0—20mA and 4-20mA current signals. It can be programmed to display voltage or current units and be mapped to user-defined scales with up to 4.5 digits of resolution. Finally, the DMR30-TC1 temperature meter accepts J, K, T, and E type external thermocouple inputs and can display in Fahrenheit, Celsius, or Kelvin with up to 0.1 degrees of measurement resolution.

“Murata’s DMR30 series of panel meters is one of the most flexible, accurate and cost efficient solutions available today. Advanced electrical design elements, packaging technology, and assembly techniques all went into its development – benefits that will have an immediate and significant impact on design engineers that face interface integration challenges every day,” said Bill Smith, Director – Product Line Management, Murata Power Solutions.

View Product Specifications for the DMR30-DCV1

View Product Specifications for the DMR30-DCA1

View Product Specifications for the DMR30-PM1

View Product Specifications for the DMR30-TC1

Murata in Brief

Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com

Subscribe to Product & Event News

Sign Up for Our Free Email Newsletter