Ceramic Capacitors FAQQWhy can’t flow soldering be utilized with chip multilayer ceramic capacitors other than 1608M(0603), 2012M(0805), 3216M(1206) in mm(inch) sizes?

A
With the 3225M(1210 inch) or larger sizes, the temperature difference between the inside and the chip surface increases, and this difference (Thermal shock) might cause cracks to occur. As a result, they are excluded from flow soldering. 
The 1005M(0402 inch) or below, smaller size chips might fall off or bridges might be formed when they are processed by flow soldering. So, these sizes too are also excluded from flow soldering. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.