Ceramic Capacitors FAQQWhat precautions are in order regarding application of adhesive before flow soldering of chip multilayer ceramic capacitors?

A
If you want to temporarily attach the capacitor to the board using an adhesive agent before soldering the capacitor, first be sure that the conditions are appropriate for affixing the capacitor. If the dimensions of the land, the type of adhesive, the amount of coating, the contact surface area, the curing temperature, or other conditions are inappropriate, the characteristics of the capacitor may deteriorate.

Please refer to the following file as it describes the adhesive application.

Caution/Notice MLCC for automotive (PDF)


<Related FAQ>
Do you take any precautions related to adhesive setting before flow soldering of chip multilayer ceramic capacitors?


We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.