Ceramic Capacitors FAQQPlease explain the MSL test conditions, including the reflow profile, described in J-STD-020.

A

Our SMD multilayer ceramic capacitors (MLCCs) were evaluated in accordance with J-STD-020 and judged as MSL(Moisture Sensitive Level)1.

There were no surface defects and electrical failures after 85℃/85%RH/168hrs moisture soak and 3-cycles reflow test described in J-STD-020.
The reflow profile called out in J-STD-020 is specified for the MSL test only.

When our MLCCs are mounted on your PCBs by a reflow process, please take into consideration all factors that may affect the soldering process including, but not limited to, the reflow profile, all solders, PCBs, other SMD products mounted on the PCB, prior to selecting a suitable reflow profile.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.