A
Yes, please refer to the following precautions to open a waffle pack.
- Lightly tap the reverse side and front side before opening to separate the components from the cavity and cover paper.
- The components may become stuck if the cover paper is electrically charged, so remove the charge with a hand holding tweezers so that the cover paper does not become electrically charged.
- Slide the cover paper to the side without lifting it up to quietly remove it.
For more details, please check the documentation.
Related terms : Silicon Capacitor(Si-Cap), Silicon IPD(Si-IPD, Integrated Passive Device)