Silicon Capacitors FAQQWhat is the relationship between BV (breakdown voltage, BDV) and recommended working voltage?

A

The withstanding voltage of a silicon capacitor is defined by the BV, there is no setting for the rated voltage, and the recommended working voltage is defined by the product lifetime and operating temperature.
Murata indicates as the recommended working voltage, the maximum DC voltage (continuously applied) at which the product is projected to have a service life of 10 years in a 100℃ environment. The maximum recommended working voltage is approximately 1/3 to 1/2 the breakdown voltage depending on operating conditions and target lifetime. For more details refer to the application note “Lifetime of 3D-capacitors in Murata technologies,” as the BV differs between products.

Swipe left or right to change screens View in landscape mode.
Murata Silicon Capacitor
Breakdown voltage
(BV)
Recommended working voltage Murata dielectric
molding technology names
Standard Type
11V 4V PICS3 SMD
30V 10 PICS3HV SMD
50V 17V PICSHV50 Vertical
100V 34V PICS3HV100 Vertical
(SMD)
150V 50V PICSHV150 Vertical

Related terms : SiliconCapacitor(Si-Cap), SiliconIPD(Si-IPD, IntegratedPassiveDevice), Breakdownvoltage(BV, BDV), ratedvoltage(RV), recommendedvoltage, workingvoltage, drivevoltage, voltagetolerance, withstandingtolerance

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.