Variable Capacitors FAQQOn the input impedance of the control voltage

A
Input impedance (Vtune –GND)
   
Vtune and GND
Circuit model
 
   
P/N
Parallel Cap.
(pF)
Parasitic Cap.
(pF)
RF signal Cut
Resistance
(Ω)
Insulation
Resistance
(Ω)
LXRW-050,056  3,300  0.5  150k  10M
LXRW-054,055  3,840  0.5  150k  10M
LXRW-053  5,760  0.5  150k  10M
LXRW-058, 059  12,800  0.5  50k  10M
Input impedance Details(Vtune –GND)


VAC consists of a capacity part and a resistor part.
The two capacitors and the resistance can be simplified between the vtune and GND.


Measurement results(LXRW19V201-058) 

The capacitance between VTune and GND is 12.8 nf * and parasitic capacitance is about 0.5 pf.

*Simulation parameters


We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.