A
Available on all products.
Refer to this data sheet.
Carefully perform preheating so that the temperature difference (ΔT) between the solder and products surface should be in the following range. When products are immersed in solvent after mounting, pay special attention to maintain the temperature difference within 100 °C. Soldering must be carried out by the above mentioned conditions to prevent products from damage. Contact Murata before use if concerning other soldering conditions.
Reflow soldering standard conditions (Example)
Use rosin type flux or weakly active flux with a chlorine content of 0.2 wt % or less.