TVS Diodes (ESD Protection Devices) FAQQPlease explain how to store TVS diodes.

A
  • Store TVS diodes in an environment with an ambient temperature of 15 to 35°C and humidity of 45 to 75%RH.
    Packing material may become deformed if the temperature exceeds 40°C.
  • Do not store them in environments with corrosive gas that includes sulfur and chlorine.

Download and check data sheets from the series page for other detailed information.

Related Links

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.