Select your region & language

Inductors FAQ Q The max. and typ. values are given for the rated current (based on inductance change / based on temperature rise). However, the max. value is lower than the typ. value in the values given. What does this notation mean?

A

Max. is the guaranteed maximum current value. Typ. is the actual ability value. The max. value is the guaranteed strict standard. Therefore, it is set smaller than the typ. value.