Shock Sensors FAQ

Characteristics

Can the strength of shock be determined?

The output of shock sensor is the amount of charge proportional to the magnitude of applied shock, it is impossible to determine the intensity alone. However the magnitude of shock is detectable by adding peripheral circuit (amplifier and comparision circuits). It is necessary to check and adjust output through actual set by defferent vibration trasmission depending on mount position or around circuit devises. 

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.