NTC Thermistors FAQQ[NC* Series] Are there guidelines for selecting NTC product numbers?

A

There are no guidelines, but please select a general product or a highly reliable type depending on the set you are considering, and select the size from the perspective of space. Select a resistance value that is easy to handle at the temperature monitoring point. XH103 (R25 = 10kΩ) and WF104 (R25 = 100kΩ) are commonly used. Determine the deviation of the resistance value from the required temperature accuracy to be measured.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.