Select your region & language

NTC Thermistors FAQQ[NC* Series] When are the various circuits used in SimSurfing?

A

It is typically used in simple circuits with NTC ground or resistance ground.
Additional resistance is used to move the maximum sensitivity and to adjust the output on the low/high side. Refer to the manual for the adjustment method.