Select your region & language

PTC Thermistors (POSISTOR) FAQQ[PRF Series] Is it possible to use PRF series with an AC circuit?

A

The rating of POSISTOR is specified by the DC circuit.
It is possible to use it with an AC circuit, but use it with an AC circuit below the commercial frequency.
If PRF series is used in a high-frequency AC circuit, there is a risk that the protective characteristics of the product may not be fully realized.