Select your region & language

PTC Thermistors (POSISTOR) FAQQ[PRG Series] Is it possible to use it with an AC circuit?

A

The rating of POSISTOR is specified by the DC circuit.
It is possible to use it with an AC circuit, but use it with an AC circuit below the commercial frequency.
If the product is used in a high-frequency AC circuit, there is a danger that the protective characteristics of the product may not be fully demonstrated.
Please contact us for detailed frequency conditions.