Select your region & language

Smart Factories of the futurePredictive maintenance

Predictive maintenance is a maintenance strategy that utilizes predictive analytical algorithms and real-time data to proactively identify areas of potential concern and provide suitable solutions. One of the key reasons for interest in predictive maintenance in a smart factory will be the cost savings it enables, which can be significant over a period of time. However, factories using this strategy will have to deal with issues such as data protection and significant capital expenditure.

Smart Factories of the future
Download Whitepaper

Find our latest Smart Factory content

Whitepaper Download

Big data and Ai

Big data and AI represent an attempt to create machines that can sense, process and act like humans, including undertaking complex tasks such as natural language processing, planning, image, object and sound recognition, and making objective business decisions. With the help of big data, for instance, manufacturers can undertake predictive maintenance in the smart factory to identify patterns or predict events that can bring significant cost savings and improve margins.

Predictive Maintenance

media object

Demand for predictive maintenance in automated manufacturing is rising due to its potential to reduce the risk of malfunction, minimize downtime, and prolong the lifespan of equipment. Smart manufacturing simplifies the maintenance process by applying advanced data analytics with condition monitoring for consumables, wear-and-tear, and performance.

These data translate into significant cost-savings for manufacturers and eliminate the need for labor-intensive, imprecise manual checking methods. In real-time monitoring, sensors are attached to machines to actively detect and obtain accurate data on the condition and environment of workers, vehicles, machinery, and facilities. They also track the levels of consumables such as lubricants or refrigerants, as well as their temperature, viscosity and other variables. Powered dashboards gather and analyze data, promptly sending alerts to key personnel if a change is detected, so that corrective actions can be taken immediately. Detailed downtime analysis and failure reports on key machines, components or process constraints are generated for a holistic view of future maintenance needs, enabling manufacturers to reduce the mean times between malfunctions and repairs.