Select your region & language

Ceramic Capacitors FAQQDo you have any cautions for measurement of capacitance?

A
When measuring the capacitance of a ceramic capacitor, it is necessary to use the correct measurement conditions indicated in the specification sheets, for example. The conditions sometimes differ according to the nominal value of the capacitance, so care is necessary. These conditions are mainly the heat treatment prior to measurement, the measurement voltage, and the measurement frequency.

For more details: