Silicon Capacitors FAQ Q What is the difference between "ULSC, BBSC, UBSC, XBSC" of silicon capacitor series for Broadband?

A

The diferrence between these series is the supported frequency. Supported frequency of each series is on the following table.

Series Description Supported frequency
XBSC Extreme Broadband Silicon Capacitor 100GHz+
UBSC Ultra-Broadband Silicon Capacitor 60GHz+
BBSC Broadband Silicon Capacitor 40GHz
ULSC Ultra-Large Band Silicon Capacitor 20GHz

Related terms : Silicon Capacitor(Si-Cap), Silicon IPD(Si-IPD, Integrated Passive Device), Ultra Broadband, 5G, Server, Datacenter, SMD, SMT, Surface Mount Device, Surface Mount Technology, High Frequency, Low Insertion Loss (Low IL)

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.