Select your region & language

TVS Diodes (ESD Protection Devices) FAQ QMounting Position of TVS Diodes (ESD Protection Devices)

A

The ESD suppression effect is higher with pattern (2) in which the TVS diode is placed at the connector (entry point).

  • Image of pattern (1)
  • Image of pattern (2)

We give an image of ESD suppression with patterns (1) and (2) below.
The value that can be suppressed by the TVS diode is fixed. It is possible to release ESD further with a CMCC or similar.

Image of ESD suppression with patterns (1) and (2)

Related Links