Select your region & language

Inductors FAQQEven though the LQH32C and LQH32P are the same size, why are the land dimensions different?

A
The dimensions differ in consideration of the Q characteristics.

<Difference between LQH32C series and LQH32P series>
LQH32P series: This series has a closed magnetic circuit structure coated with a magnetic particle resin.
Therefore, the generated magnetic flux does not leak out so easily, and is not affected by the land.

LQH32C series: Since there is more magnetic flux leakage in this series compared to the LQH32P series, the Q characteristics may deteriorate after mounting due to affects from the land.
Therefore, the land dimensions were reduced to decrease the effect from the land.