Select your region & language

Power Products FAQ QMalfunctions occur depending on the model of the power sourcing equipment (PSE) connected to the powered device (PD).

A

Detection failures may occur depending on the grounding condition of the AC line of the PSE connected to the PD and the equipment connecting to the PD.
Therefore, we recommend using a 3-core cable to ground the AC line of the PSE and the equipment connecting to the PD.

Note
We have confirmed that the products starts up even with a 2-core cable. However, commercial power supply noise may be superimposed on the detection waveform and detection failures may occur.
Swipe left or right to change screens View in landscape mode
Example of a PoE power supply device connection Fig. 1: Example of a PoE power supply device connection
Swipe left or right to change screens View in landscape mode
Actual waveform Fig. 2: Actual waveform