Select your region & language

Power Products FAQ QWhat will happen if the external capacitor is smaller than the minimum capacitance value?

A

In addition to the output ripple voltage increasing, abnormal oscillation may occur depending on the operating conditions.
Therefore, please design and use the system so that the capacitor is equal to or greater than the minimum capacitance value.