Select your region & language

Power Products FAQ QAbout the handling of products that require Moisture Sensitivity Level (MSL) management (MonoBK™ series etc.)

A

You need to store products that require MSL management in a desiccator after opening the package.
If you manage the moisture proofing for these products in a desiccator, you can extend their floor life indefinitely.
Do the following when using these products:

  • Remove the product from the desiccator
  • Open the package
  • Cut the product from the reel
  • Seal the package

If the floor life is exceeded, you will need to perform a baking process to reduce the moisture.
The baking conditions are as follows. This process can reset the floor life.

  • 125°C for 48 hours or 40°C with an RH of 5% for 67 days
  • Baking is possible up to two times