Select your region & language

AMR Sensors (Magnetic Sensors) FAQ QWhat are the advantages of magnetic sensors?

A

Magnetic force lines are invisible.

Magnetic force lines are not absorbed by plastic, aluminum, copper, and other non-magnetic bodies and pass through to the opposite side. Magnetic sensors use these features to enable detection.

The advantages can be easily utilized in the following usage situations:

  • Notebook computer open/close detection and security device activation settings (Switch location is not visible.)
  • Gas, water, and other rotation detection (structures where sealing is important)
  • Power switches of wearable devices (the sensor unit requires current, but the sensor is easily adaptable into a waterproof structure)