Select your region & language

CO2 sensor FAQ QCan we use these sensors in the high-humidity and sulfur-fumigated environments of greenhouses and plant factories or in darkrooms?

A

These sensors have a proven track record of use in greenhouses with high humidity (80 to 90% RH). They can also be used in sulfur-fumigated environments. However, this will affect their lifespan, so such use is not covered by the quality guarantee. They can even perform measurements without being affected in principle in darkroom environments.