Select your region & language

Infrared Sensors FAQQHow we can do soldering for a Pyroelectric infrared sensor?

A
The soldering conditions for them are as follow. 
<LEAD Type>
Please perform the soldering of the terminal with an iron point solder.
Please mount the soldering of the terminal as quick as possible. Specifically, please go in the range of follows.
 •Iron point temperature:350゚C max.
 •Time:
  Terminal length from stem 1 to 3mm : Less than 3.0 sec by terminal.
  Terminal length from stem Over 3mm : Less than 10 sec by terminal.

<SMD Type>
The SMD type can be soldered with reflow soldering.

Both types can not be soldered with flow soldering(wave soldering).