Yes, it is influenced.
When air blows on the pyroelectric infrared sensor, a sudden
temperature change occurs on the surface of the sensor and the pyroelectric ceramic reacts to the
temperature change, and an output may occur.
For this reason, use in a location where it is not
influenced by air flow (no direct air flow).