Select your region & language

NTC Thermistors FAQQ[NC* Series] What is B constant?

A

This is the NTC thermistor constant calculated from the resistance of the two temperatures, and represents the rate of change of the resistance. We define in 2 points, 25°C and 50°C.