Select your region & language

NTC Thermistors FAQQ[NXF Series] What happens if the maximum operating current is exceeded?

A

The maximum operating current is the current that self-heats up to 0.1°C when applied to the NTC thermistor alone. If the current exceeds the maximum operating current, self-heating will exceed 0.1°C, affecting the detection accuracy. Please check the temperature error with the actual machine.