Select your region & language

NTC Thermistors FAQQ[NXF Series] What should be noted when measuring the resistance of the NTC thermistor?

A

NTC thermistors have a characteristic that the resistance value changes with temperature change. Therefore, it is important to minimize the fluctuation of the ambient temperature when measuring the resistance.
The following describes the points to reduce the fluctuation of the measurement environment temperature.

Point 1
Measure the resistance value so that you do not touch the device or board with your hands.
Point 2
Set up a thermometer to indicate the ambient temperature of the resistance measurement space.

The following are precautions for measuring NTC thermistor resistance.