Select your region & language

PTC Thermistors (POSISTOR) FAQQ[PRG Series] What is the maximum voltage when two PRG series units are connected in parallel?

A

The maximum voltage does not change even if multiple POSISTORs are connected in parallel. Do not exceed the maximum voltage.