Select your region & language

PTC Thermistors (POSISTOR) FAQQ[PRG Series] Will it trip even if holding current is applied?

A

The rated holding current value is set on our standard circuit board and in the mounting state.
If the heat dissipation conditions in the actual use environment differ significantly from our conditions, POSISTOR may trip by even hold current.