Select your region & language

PTC Thermistors (POSISTOR) FAQQ[PRG Series] How to store the parts before mounting?

A

Observe the following conditions.

  1. Storage Temperature/Humidity
    Ambient Temperature: −10 to +40°C
    Relative humidity: 75%RH or less (no condensation)
  2. Storage period: First in, first out and use within 6 months after delivery.
  3. After opening, please reseal the minimum package or store in a sealed container containing desiccant.
  4. Store in a place that is not exposed to direct sunlight or special gases such as sulfur or chlorine.