Select your region & language

Ceramic Resonators (CERALOCK) FAQQDoes CERALOCK have orientation?

A
CERALOCK has orientation. Please connect input terminal(1) to XIN of IC, output terminal(3) to XOUT.
When putting components in direction where frequency marking is readable, terminal number shall be (3)(2)(1) from left.

Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
What are the meanings of the Marking?
Q.
Is there any problem if CERALOCK is mounted in opposite direction?
Q.
Why does frequency correlation occur when CERALOCK is mounted in opposite direction?